Tool/software:
Hey pros!
The idea is to use a switch to swap between two charge currents. Charge current #1 = 1A , Charge current #2 = 2A , for example
Does BQ25308 allow changing of the resistor dynamically? Or is this only read upon startup?
The next layer: could a switch cause the BQ25308 to reset while it reads the switch as open? Via the 8.3.4.4 ICHG Pin Open ; for the "break before make" switches
Thanks!
Cameron