Other Parts Discussed in Thread: GPCCHEM
Tool/software:
The BQ28Z610-R1 is configured with high temperature step-down charging. The full charging voltage is 8.648V at 0~45℃ and 8.4V at 45~60℃.
The battery starts to charge at 30℃ with 8.648V 5A, and after a period of time, the battery temperature starts to rise, when the battery reaches 46℃, the RSOC is 70%, then the voltage reduction charge begins, and the charger starts to drop to 8.4V, 1152mA current to charge the battery, but when the charge reaches 91%, the full charge cut-off condition is reached.At this time, RSOC jumps directly from 91% to 100%, is there a way to make RSOC not jump, but smooth to 100%?