This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5177: Meed LM5177 Simplis model

Part Number: LM5177


Tool/software:

Hi eveyone,

I'm going to design and implement a bidirectional circuit with LM5177,

could you share the Simplis model of LM5177 controller?

Thanks

Regards,

TSUNG-HUI CHEN

  • Hi Tsung-Hui-Chen,

    I would recommend to start the design with the newer version of this device: LM51770 (identical footprint and features but better performance, e.g. input and output voltage range)

    The Simplis Model is only shared under NDA. Please contact your local support or sales channel to check if there is an NDA or to request the setup of one. Then you can also request the Simplis Model over this channel.

    Best regards,

     Stefan