Part Number: TPS563203
Tool/software:
Hi i am using TPS563203 DC-DC CONVTER TO POWER EC200 I WANT OUTPUT VOLTAGE 3.8V AND CURRENT REQUIREMENT IS 3A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS563203
Tool/software:
Hi i am using TPS563203 DC-DC CONVTER TO POWER EC200 I WANT OUTPUT VOLTAGE 3.8V AND CURRENT REQUIREMENT IS 3A
Hi,
Hope you're doing well I am using TPS563203DRLR DC-DC converter IC in IOT project where I need to power
EG91NALGATEA-512-SGNS I need output voltage +3V8/3A
schematic which I designed is ok please check.
Input voltage:9-16V DC
Rated Input Voltage:12VDC
Output Voltage: +3V8
Output Current:3A
Dear Shahrukh,
Pls add a 18pF Cff (parallel with top feedback resistor). Thank you!
BRs
Lucia
Dear Sir,
You can keep what you used in the schematic. Or you can refer to datasheet LC table.
Thank you!
BRs
Lucia