Tool/software:
Hi,
I have multiple instances where a TPS7A2030PDBVR output is latched shut off while the EN pin in high (equal to VIN 4.2V).
When I toggling the EN pin low then high the regulator resets and then works fine.
I can find no damage or reasons. I do have larger than recommended capacitor loading (300uF). I have several 0.1uF ceramics nearby as well.
What situations could cause the regulator to shut down with Vout = 0 and EN = Vin? I have tried brief shorts and higher than recommended Vin and can not reproduced the failure on demand.
Thanks,
Doug