This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5171: Is IMON 'bidirectional', similar to ISET, when in Boost FPWM mode?

Part Number: LM5171


Tool/software:

When ISET goes below its 1V offset when LM5171 is in Boost/FPWM mode, which makes buck operation happen as shown in datasheet Figure 7-28 (and on the front page), does IMON also go below its 50uA offset to indicate reverse load current? (When CFG pin is used to set IMON to measure Load Current rather than inductor current)