Tool/software:
I have a question related to using two TPS25751 controllers in a single design that has neither a battery nor battery charging capability. A high-level block diagram is given below:

The intent for this design is to allow a user to connect a USBPD certified power supply into either port and have the secondary port be available for data and potentially sourcing power. Prior to being powered up, both TPS25751 devices will be configured in dead battery mode.
Looking at the TPS25751 data sheet, figure 8-11 shows the following:

Since the TPS25751 controllers are starting in dead battery mode, initial power will come from VBUS and, then it will be up to the embedded controller to clear the dead battery flag.
Question 1: Is clearing the dead-battery flag equivalent to closing the RLDO_3V3 switch in figure 8-11 above?
Question 2: Once the system powers up through the first TPS25751 controller, there would be power coming in to VIN_3V3 and not VBUS. However, if the dead battery flag is not cleared, does this prevent the TSP25751 controller from powering up?
Thank you,
William