Hello,
I want to insert the coil circuit as one of the layers of the PCB is it possible?
What is the minimum inductance of the coil (for 100 - 200mA)?
Can I get examples of these coils?
Thank you,
Ido
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I want to insert the coil circuit as one of the layers of the PCB is it possible?
What is the minimum inductance of the coil (for 100 - 200mA)?
Can I get examples of these coils?
Thank you,
Ido
PCB coils are possible, we are testing some versions. A shield will be required behind the coil.
The inductance should be between 10uH to 15uH, this is with the complete stack up using WPC test fixture and battery.
Can you describe the size of coil you will use or area you have available for the coil?
Hi there,
is the shield behind the coil strictly necessary?
Did you find some geometrical suggestions for an board are of around 25x25mm?
Thanks in advance,
Reinhard
Reinhard,
The coil shield for the bq51013B is required. The shield is used to contain and optimize the magnetic field created by the transmitter. Without the shield, the energy created by the power transmitter field would be absorbed by other material and could cause heating or other unwanted results.
Regards,
Dick
Thanks Dick, this is relatively the same scenario described by Ido at the beginning of this post.
Do you have any recommendations to design a PCB coil (in a 25x25mm area) to charge a 150mAh Lipo Battery?
Thanks,
Fernando
Fernando,
I have no specific recommendations, but some things to be aware of. In general, a PCB coil will be lower in efficiency than a standard coil. Your charge current will be relatively low so this may not be a huge impact. The resonant capacitors must be tuned to the specific coil you are using. Work closely with the PCB coil manufacturer to understand their process and what to expect from the inductance and resistance.
Regards,
Dick