This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8864-Q1: turn each channel on/off individually

Part Number: LP8864-Q1
Other Parts Discussed in Thread: LP8863-Q1

Tool/software:

Hi,

With an input voltage of 3.3V to 24V, approximately 20 LEDs are connected to the output stage. It is planned to be controlled by I2C and SPI, and a current of about 50mA per channel will be applied. I am considering the LP8864-Q1 or LP8863-Q1, but is it possible to turn each channel on/off individually? If not, could you recommend another IC?

Best Regards,

Nishie