This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65994AD: ADCIN1 and ADCIN2 settings

Part Number: TPS65994AD


Tool/software:

When setting ADCIN 1:7 and ADCIN 2:5,
Is it set to 5V / 3A output?
Does 'PD' communication send SOUCE CAP and support the operation of EMCA CHECK or DP when set up as above.

I'm designing a USB4HOST controller.
Since there is a limit of current, I want to set ADCIN to limit the output current.
When setting up 5V/3A via ADCIN,
Is there a problem with PD communication?

Thank you.