Part Number: LM5170
Other Parts Discussed in Thread: LM5171
Tool/software:
Hi experts,
I'd like to use the LM5170 to drive the GaN FETs. Due to the PWM output voltage of LM5170 is 9~ 12 V, but the GaN FET needs 5 V.
Therefore I'm about to use the GaN driver LM1205 to transfer the voltages, and then the high-side boot-strapped function need to be disabled.
Just want to make sure whether my design is correct?
"HB1 and HB2 pins connected to the VCC/ SW1 and SW2 pins connected to the ground."
The schematic is shown below:

Hopefully to hear your feedback soon.
Best,
Lucien