Other Parts Discussed in Thread: LM25184,
Tool/software:
Hello,
I have a question based on the transformer selection for the LM25184-Q1. We want to create two outputs of about 7V (350mA) and 15V (30mA) from inputs ranging within the LM25184 limits (about 10V - 20V).
Based on my understanding of the circuit, the transformers suggested in the datasheet for dual outputs (Würth Electronik 750318704 or Coilcraft ZA9675-BE) should suffice for the same, based on the external components being adjusted for the required voltages and currents, correct? Or do I miss something here?
Thanks and best regards,
Akhil