Part Number: TPS25751
Other Parts Discussed in Thread: TPS25750, BQ25792,
Tool/software:
Hello,
We are using a battery charging PCB designed with the TPS25750 and BQ25792 in our early products. Now, we want to use new version TPS25751. However, our existing patch does not seem to work with the new IC. We understand that we can generate a new patch using the Application Customization Tool, but this would result in two separate patch files, one for the TPS25750 and another for the TPS25751 which means an configuration necessity.
To ensure that the correct patch is loaded into the EEPROM, we need a way to determine which IC is present on the board. Is there a specific register that provides an identifier for TPS?
Thank you.