Other Parts Discussed in Thread: TPSM82822A, TPSM828512
Tool/software:
Hello,
I am evaluating the TPSM828302 to provide core power to a Spartan 7 FPGA with the following requirements:
1. Vin = 4.5V to 5.5V (Within the input voltage range of this device as shown on datasheets).
2. Vout = 1.0V +/-50mV (Within the output voltage range of this device as shown on datasheets).
3. Iout = 2A maximum.
4. FPWM (CCM) Mode Only.
When I use WEBENCH Designer with the above Vin, Vout, and Iout, I get Design cannot be created. If I increase Vout to 1.1V, then WEBENCH Designer is able to create a design.
My questions:
1. For 1V output at 2A, is Ton too low for WEBENCH Designer to create a design?
2. What is the minimum Ton for this device that must be met since I can not find this on the datasheets?
3. The datasheets list a Typical Fsw = 2MHz. What are the Min and Max Values of Fsw?
4. In FPWM (CCM) Mode, is Fws fixed or varied based on Iout?
5. I find a similar device (TPSM82822A) and I am able to use WEBENCH Designer to generate a design for 1V output using this TPSM82822A device. Can you tell me the differences between TPSM828302 and TPSM82822A?
6. Any recommendation for other devices that meet my requirements above and are recommended for new design?
Thank you very much for your support.
Regard,
Long Nguyen