Tool/software:
Hello,
I am an FAE at a distributor that handles TI products.
I received an inquiry from my customer about the LM27762.
The specifications are as follows.
I have a question about the "8.2.2.5.3 Flying Capacitor" section of the datasheet.
The recommended value for the flying capacitor is 0.47uF or 1uF, but would there be any problems if I connect a capacitor with a larger capacity of 4.7uF?
(Specifications)
VIN:5V
VOUT:±4.5V
IOUT:1mA
Best regards,