This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2776: Internal MOSFET Structure

Part Number: LM2776


Tool/software:

Hi all,

About internal MOSFET Structure of this device,  This device is a DCDC with intergrated FET and uses an internal MOSFET.

1) Is this MOSFET a high-current power MOSFET?

2) Is this MOSFET a vertical structure or horizontal structure?

I think it is not power MOSFET because it has a low current value of 200mA.

I would appreciate it if you could let me know.

Best Regards,

Ryusuke

  • Hi Ryusuke,

    Thanks for using E2E.

    Please take a look to the description in the data sheet, page 12.

    Best regards,
    Sepp

  • Hi Sepp,

    Thanks for the confirmation. I read it. I would like to know more details about the ''internal MOSFET'' mentioned in this Description.

    1) Is this MOSFET so-called "power MOSFET"?

    If it is designed to handle high current, it is a power MOSFET. I would be happy to know the rating and Rdson details of the MOSFET.

    2) Is this MOSFET a vertical structure or horizontal structure?

    MOSFET structures can be roughly divided into the following. In this case, which is it?

    Best Regards,

    Ryusuke

  • Hi Ryusuke,

    The data you are asking for are TI Confidential. I'm not allowed to provide to you, sorry.

    Best regards,
    Sepp