This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1641: used in a Low Side Switch Application

Part Number: TPS1641

Tool/software:

I am looking at this part as an e-fuse for a client and their application doesn't fit the normal use case for devices such as these. It is 12V and 24V applications, but this device would be in the Low Side Switch leg of small fluid pumps. This puts the e-fuse at ground when the pump motors are turned on. The pump motors are sourced with either 12V or 24V. I'm not sure how well these devices will work i that application. This would have the IN of the device connected to 12V/24V through a pump motor with the OUT connected to ground through a switched FET.

Could someone please give me a call to discuss these devices. 314 277 4570.  I am in the central time zone, but I answer my phone from about 6:00 AM to about 10:00 PM

Thank you.

Best regards,

Mike Boyle