Other Parts Discussed in Thread: BQ25750, BQ34110
Tool/software:
Hi, We are exploring the suitability of BQ25756 in Solar Tracker system. Below are the specifications:
1. Input power 80W/100W PV panel, VMP=33V & VOC=43V
2. Battery 4AH or 6AH, LiFeO4, 8-cell
3. System load (Battery Charging + DC Motor + MCU with associated sections) ~100W
We would like to understand when system demands full power (100W) and if the PV source is not capable to provide all power, will BQ25756 able to source required extra current from battery? Can you please provide some insights of the operation?
-Satish