This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM61430-Q1: IC active mode and shutdown mode

Part Number: LM61430-Q1

Tool/software:

Hi Team,

In LM61430-Q1 regulator datsheet,

it is mentioned that enable pin below 0.4V device in shutdown

enable pin above 1.263V device in active state

than what about the state in between 0.4 to 1.263 V ?

Kinldy clarify

Regards,

Aravind D