This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS653860-Q1: Whether DCDC can output 3.3V and 5V?

Part Number: TPS653860-Q1
Other Parts Discussed in Thread: TPS650362-Q1

Tool/software:

Hi Expert,

Customer is seeking a PMIC, which DCDC output voltage is 3.3V & 5V, output current is 1A. While I find TPS653860-Q1 DCDC's min output voltage is 4.3V. Could you help check if DCDC can meet the 3.3V output requirement?