Tool/software:
Hello,
one short question to the TPS54824 - Is it possible to synchronize three of them using
the RT/CLK Pin ? - Or does the TPS54824 only support SYNC input but no SYNC OUT.
MfG
Frank
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
one short question to the TPS54824 - Is it possible to synchronize three of them using
the RT/CLK Pin ? - Or does the TPS54824 only support SYNC input but no SYNC OUT.
MfG
Frank
Hi Frank,
TPS54824 only supports sync in on the RT/CLK pin. Looks like you are planning on multiphase operation - is that correct? You may need to add the logic to control the clock externally on each of your 3 ICs to get the operation required if so.
Thanks,
Amod