This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54260-EP: Failure Protection Mechanism at higher temperature

Part Number: TPS54260-EP

Tool/software:

Hi,

I'm using regulator TPS54260MDGQTEP which is having a shutdown temperature of 182 Degree C.

1. Is it telling about the junction temperature or ambient? 

2. Other query I have regarding the temperature range if the junction, operating storage is given as 150 Degree C, what will be the IC behavior between 150 - 182 Degree C.

I'm doing a worst-case thermal analysis where the IC case temperature is going to 183 Degree C (in software simulation). So, I need all the high temperature behavior of this IC to have more substantation in my report.