This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74700D-Q1: 100A battery polarity

Part Number: LM74700D-Q1
Other Parts Discussed in Thread: LM74500-Q1

Tool/software:

Hi,
I need ideal diode for 12V device (because of reverse polarity protection = I need to NOT switch-on the device when someone connect red wire to GND and black wire to +12V).

There will be 100A. Is is possible to use  LM74700D-Q1 with multiple FETs (4x DMT6005LPS-13)?
Or could recommend me another (80A) 100A FET?


LM74700D-Q1 works well in my design...this is the reasony why I would like to modificate him...
If there is better circuit for my design, I can use it.

Thanks!