Other Parts Discussed in Thread: LM70880-Q1
Tool/software:
We configured LM73100 as priority mux (see schematic) but observed here different behavior than expected.
We tried this test scenario:
1) Turn on VIN2, VIN1 is off, at the output is 12.1V as expected
2) Turn on VIN1, VIN2 is keept ON, at the output is 12.3V as expected
3) Turn off VIN1, VIN2 is keept ON, at the output is 12.1V as expected
4) Turn on VIN1, VIN2 is keept ON, at the output is 12.3V as expected
5) Turn off VIN1, VIN2 is keept ON, at the output is 0V, but was expected VIN2 = 12.1V
Looks like secondary path went to Fault condition during step 5. Why that happened?. After step 5, we must do power cycle on both power supplies VIN1 and VIN2 to make output again working.
Could You please explain that. Thank You.
Martin / Kontron