Part Number: TL1451A
Other Parts Discussed in Thread: TL1451
Tool/software:
Hi team,
I have another question about TL1451A.
We need to detect TL1451A fail.
My idea is that to monitor the comparator output signal if it is stuck high or low.
As long as the output signal is at set clock signal, it is not a failure.
If the output signal frequency falls below a certain frequency, TL1451A is determined to be failure.
Q1
To what extent can TL1451A failures be detected using the above method?
What failure modes are there that cannot be detected?
Q2
What would be an appropriate frequency for determining a failure when the clock setting frequency is 100 kHz?
Thanks