Tool/software:
Hi expert
I have a question about learning cycle sequences.
Check the process below and verify if a reset command is needed.
<learning cycle sequences>
1. Write to Update Status = 0
2. Discharge to Empty
3. Rest 5 Hour
4. IT Enable (Update Status = 4)
5. Send Reset command (0x41) and then check DOD0 is same as QMaxDOD0
6. Charge to Full (FC = 1)
7. Rest 2 Hour
8. Discharge to Empty
9. Rest 5 Hour
10. Check Update Status = 6
11. IT disable (Update Status = 2)
12. Clear cycle count
13. save golden image