Tool/software:
I have received TPSM365R6FEVM from Digikey and identify the current consumption from Bench PSU read 14mA from 24V which is deemed excessive compare to datasheet which quoted less than 10uA unloaded current even in FPRM mode. When EN jumper to OFF, it drop to 0mA. When EN jumper to ON, it read 14-15mA. No RLOAD is connected. It seem to be functional with RLOAD test.
Nothing in the TPSM365R6FEVM document mentioned expected current.