Part Number: TPS25980
Other Parts Discussed in Thread: TPS1663, TPS2663
Tool/software:
Hello,
we are designing a power supply unit for 24V with unknown load currents.
Since we need to comply with IEC61010-1 we want to connect two TPS25980 in series and set the current limit to the maximum possible value of 6.25A.
(9.4 b) 3) A regulating network limits also in SINGLE FAULT CONDITION)
The datasheet mentiones a accuracy for ILIM. At 6.25A the accuracy is ~11%. Is this to be understood as a deviation, so that in order to reliably limit the current to 6.25A, I have to set the limit to 5.56A?
Many thanks in advance.