Tool/software:
Hi AE,
Step1. PDFW is set to Source Only.
Step2. When shutdown system, EC will write 0x28 register to 0x03 disables port A and portt B to stop charging the device. ( Port A and Port B can not charge )
Step3. When the system power on, We found OS will send PPM_RESET and Port A could charge to device.
I have two questions to ask:
1. If I send PPM_RESET only to Port A, will it affect both Port A and Port B's registers, or only the Port A register?
2. After the PPM_RESET command by EC, which registers will be reset? Reset as default FW?
Best Regards