This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24103A: Looking for a charger IC supports 2S1P battery pack

Part Number: BQ24103A
Other Parts Discussed in Thread: BQ25750

Tool/software:

This BQ24103A charger IC supports only 20V and 2A,  

But we are looking for charge management IC for 2S1P Li- polymer battery.

The charger IC should support following

Input voltage: 8-36V,

Load Current: 10A  

Function: It can effectively switch the power from main input(8-36V) to battery when the main power supply is unavailable