Other Parts Discussed in Thread: CSD85301Q2
Tool/software:
Hi team,
I help customer to post this question due to he can't post a new post to the E2E Design Support Forum.
This is a question about the circuit of the "TI Designs: 50mA Wireless Charger Booster Pack" using the BQ29707.
The battery protection circuit for the coin-shaped Li-Ion rechargeable battery of this circuit is "current Limit 100mA".
Question 1. Is it correct to understand that in order to achieve "current Limit 100mA", this circuit fine-tunes the constants of R18(221 Ω) and R19(2.21k Ω) compared to the circuit in the specification sheet, and adds "R20(0.82 Ω)"?
Q2.What is the constant calculation formula for R20 (= 0.82 Ω) that was added to achieve "current Limit 100mA"?
The FET is CSD85301Q2.
Thank you.
Regards,
Frank