Part Number: LMR51610
Tool/software:
Hey,
I was wondering if someone could check over my schematic and layout to see if there are any improvements that may help the operation of the device and/or reduce EMI. Th egoal is a 5V ouput to power a MCU and a CAN transeiver. There is 2 voltage sources and 4 wake up sources. VIN is always active from a lead acid but it looks like Qc is super low when no enabled? The 4 wake up inputs (5-28V) that come into the PCB are fitlered and they all put through a diode and when any are on then the regulator starts and turns on the MCU/PCB. DOes this sounds and looks correct? Have I made any obcious issues? This is L1, L2 and L3 are both solid GND planes that are stitched through.
Thank you in advance!