Other Parts Discussed in Thread: TPS65994
Tool/software:
PJT setting Multiport Sink Policy as "Highest power" and Auto Neg Capabilities Mismatch Power as "45W"
Plugging a 15W adapter into the first Type-C port without proper power delivery is a normal phenomenon.
However, when a 30W adapter(any small than45W adapto also) is then plugged into the second port, the 30W adapter starts supplying power.
which PJT configure need check or patch FW need update(TPS65994_F909.12.17 is used)