Tool/software:
Hello guys,
One of my customers is considering using LM5155 for their new products.
At this moment, they have the following questions.
Could you please give me your reply?
Q.
They calculated inductor value using SNVC224 — LM5155/56 Boost Controller Quick Start Calculator.
The parameters they used are the follows.
VIN(Min/Typ/Max)=3.0/3.4/3.7V, VOUT=12V, IOUT(max)=3A, Fsw=460kHz,
Estimated efficiency=90%, Ripple current=20%
Then the calculator result of inductor value was 1.364uH.
Also they calculated the inductor value using the equation No.5 in the following document too.
SLVA372D: Basic Calculation of a Boost Converter's Power Stage
https://www.ti.com/lit/an/slva372d/slva372d.pdf
The equation No.5 result was about 2.5uH.
They think the calculator, SNVC224 inductor value result is too small
and SLVA372D result is reasonable base on their experience.
The followings are their questions.
1. Which result is better to use?
2. Why is inductor value result of SNVC224 calculator different from the result of SLVA372D?
Your reply would be much appreciated.
Best regards,
Kazuya.