Tool/software:
Hi support team,
Is it recommended to use the remote sense function only with loads on the same board?
Can it also be used with loads on a different board?
Regards,
Dice-K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi support team,
Is it recommended to use the remote sense function only with loads on the same board?
Can it also be used with loads on a different board?
Regards,
Dice-K
Hello Dice-K,
In general, the remote sense is not bound to the same board. It should connect to the lowest impedance point of the load, usually at the capacitors close to the load.
The issue is in the parasitic impedance of the connection. In many cases, the connectors and cables add to much resistance and inductance to the sense lines. This can cause instability in the regulator and requires close attention to the parasitics and measurements of the finished system.
For this reason, we recommend to place the regulator on the same board as the load.
Regards, Werner