This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B86-Q1: Load transient characteristics

Part Number: TPS7B86-Q1

Tool/software:

For TPS7B8633BQ, do you have specifications or data for VOUT = 3.3 V, IOUT = 0 mA to 375 mA, slew rate = 0.1 A/µs or similar condition?

(I found some data for slew rate=0.1A/us in datasheet but IOUT is smaller than my usage condition.)

  • Hi Yang,

    It looks like the data we have that most closely matches your test conditions would be the 0mA to 500mA 1A/µs data shown in Figures 6-24 and 6-25. Overshoot and undershoot for this data is likely to exceed what your use case will experience. The 150mA to 350mA 0.1A/µs test data shown in Figure 6-23 should help provide lower bounds as well. 

    Best Regards,

    Alex Davis