Tool/software:
Hi Team,
Could you help to check if TPS7A4201 can fulfill the following requirement?
- Vin=16V-20V, Vout>15.4V, Iout=35mA
- Vout_drop<300mV under T=80°C

If not, could you help to suggest another part which can fulfill the above conditions? Thanks.
BR.
Frank