This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25983: TPS281C30B or TPS25983?

Part Number: TPS25983


Tool/software:

Hello,

I want to enable/disable a power supply for a pump (24V/3A continuous with peak current of 6A) and also have a current protection to automaticly disable the supply if the pump draws too much current (>7A).

I'm not sure which component will be better for my application, the TPS281C30B or TPS25983. Indeed even if these components are not in the same category it seems they do similar things.

Can you help me please?

Romain

  • Hi Romain,

    Primary difference between them is the type of loads you can control with them.

    eFuse (TPS25983) is suited for resistive or capacitive loads whereas High side switch can also support inductive loads. I hope this helps you in deciding the part.

    Best Regards,
    Arush