This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25751EVM: Write file to EEPROM

Part Number: TPS25751EVM


Tool/software:

Hi team,

I would like to write the settings made by EVM to EEPROM and run it without CPU.
Is the file to write to the EEPROM okay with the file created from Generate full flash binary?
The output file does not seem to match the register information, so I am wondering if writing this file will work without problems.

Best Regards,
Ryu.

  • Hi Ryu, 

    Is the file to write to the EEPROM okay with the file created from Generate full flash binary?

    Yes that is correct, the full-flash binary is intended to be loaded into a EEPROM. 

    The output file does not seem to match the register information, so I am wondering if writing this file will work without problems.

    The binary file integrates the configuration settings through the GUI with the internal PD firmware for a complete PD image. 

    Let us know if you have any further questions or concerns! 

    Thanks and Regards,

    Raymond Lin