This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792: Is BQ25792 suitable for removable series 18650 batteries

Part Number: BQ25792
Other Parts Discussed in Thread: BQ29209, BQ25798,

Tool/software:

Hello,

We are planning to design a bms for 2 series 18650 batteries which are removable from the system separately. Because of that  each cell can be accidentally inserted in reverse polarity. After each cell we will add reverse polarity circuit but I am not sure if the IC is suitable for this?  And also we are planing to use BQ25792RQMR with BQ29209DRBT. Do you have general advice for the situation where two batteries have to be removable?

Thank you