Tool/software:
Hi,
Do you have any data regarding the internal resistor divider at the sense pin which set the threshold voltage?
BR
Oscar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
Do you have any data regarding the internal resistor divider at the sense pin which set the threshold voltage?
BR
Oscar
Hi Oscar, Thanks for your question!
Unfortunately I'm unable to share that information. But you can back calculate it based on the sense pin information from the datasheet.
Hope this helps!
Best,
Sila Atalar
Hi Atalar,
It is not clear to me how can I calculate it from the datasheet.
Can you please show me?
Thank you
Oscar
Hi Oscar,
V = IR.
Please find the Isense information in below.

The resistor values is not guaranteed since the trimmed resistor values vary device to device. To do back calculation, please use the typical (25C) value.
For example:
SENSE pin voltage/ SENSE current = 42V/1.35uA = 33MOhm
this way you can expect the resistor will be in ~10 Mohms range.
Hope this helps.
Best Regards,
Sila