Tool/software:
Hi,
I have two questions about recommended component value in the data sheet of TPSM86325X.
In table 8-2, R5 and R6 are selected so that the resistor flows 20uA when the output voltage is 2.5 V~10 V, and 60uA when the output voltage is 0.8~1.05 V.
1, Please tell me the reason why you chose 20uA and 60uA.
2, I am worried about malfunction due to noise, etc. Can the current be increased if the current consumption is not concerned?
Best Regards,
Hyodo