Other Parts Discussed in Thread: BQ24232, BQ25188
Tool/software:
Hello,
For a small portable device I need to select a charger that could charge a 300mAH LiPol battery from a USB connector.
I need that the charger controller could have a Dynamic Power Path with a SYS output separated from the battery pin. Someone suggested me to use the bq24232 and it fufills all these specs.
However, and without Vin connected, I need that the chip disconnects the battery when it is on a shelf for a long time and its voltage drops below a voltage value (UVLO), and in a way that could consume microamps or less. This would be a protection for overdischarge of the battery. I have seen a UVLO in the pdf of the bq24232 but it refers to the Vin voltage and not to the battery voltage. I have not been able to see that the bq24232 isolates the battery when its voltage drops below a voltage.
Please, could you confirm me that the bq24232 has not this mode for protecting over discharge? What does the chip when supplyting the LiPOl battery voltage to the SYS output this voltage drops below 2.8V or 2.6( (for example)?
Thank you very much in advance.
Regards,
Joel