This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650: BQ24650

Part Number: BQ24650

Tool/software:

Hello,

I’m encountering issues integrating the BQ24650 into my MPPT board. I followed the application circuit from the datasheet and also referred to the bq24650EVM evaluation board as a guide.

For the MPPSET voltage divider, I used 499kΩ and 36kΩ resistors to set the desired voltage of 17.8V.

However, when I measure the input voltage (Vin), I’m not seeing the expected 17.8V. Instead, I'm getting a higher voltage around 20V or 21V from the solar panel.

As for the VSYS, VOUT, VREF, and VREGN voltages, my measurements align with the values provided in the evaluation board datasheet.

Test and Validation made:

  • Vref = 3.3V 
  • VMPPSET ≥ 1.2V
  • VCC  > SRN 
  • VREGN = 6V 
  • VOUT = 16.5V (battery disconnected); VOUT = 14.4V (battery connected)
  • D4 → ON → charging

Calculations:

  • VMPPSET = 17.8V = 1.2V * (1 + R17/R19)
    • Where R17 = 499K and R19 = 36K
  • VOUT = VBAT = 16.5V = 2.1V * (1 + R13/R15)
    • Where R13 = 820K and R15 = 120K

How can I resolve this issue?

Thanks in advance!

  • Hello Yahia,

    For the MPPSET voltage divider, I used 499kΩ and 36kΩ resistors to set the desired voltage of 17.8V.

    17.8V is the min value, if the solar panel can not suppport the required power, the input voltage will decrease to 17.8V, when it reaches that voltage, it will maintain this voltage by reducing the charge current.

    How can I resolve this issue?

    If you apply a bigger load, you should see the input voltage decrease down to 17.8V

    Best Regards,

    Christian.