Tool/software:
Hi,
We are using this integrated circuit as a solid state relay operation. However, when the power source is active, which is high, IC couldn't manage to run the gates. Also, when the load is active it is again failed to run the gates. It properly works only if the IC is first started then the power source, load is started.
I observed these from the evalboard of TPSI31xx-Q1. Is this a fault or is there a any way to solve this issue.