Other Parts Discussed in Thread: BQ25308, BQ25185, BQ25606
Tool/software:
Hello
I'm looking for a IC charger (lithium polymer ) to recharge 1 cell.
I have specials needs:
Power at the input of the charger is regulated at 5V / 2W, by a DC/DC converter OR By USBC 15W (optionnal)
IF powered by the DC/DC, the system load has to be disconnected while charging , because the system load may consume more than 3W
Power path is needed to switch off or ON the system load, the power path can whistand at least 2A in the system load
Status of the battery is required
Can you advice me plz
thx