Tool/software:
hi Team,
my customer want to use TPS70345 device at 3V3/0.5A, 1V2/1A output use case with 5V input, it is around 3W, would you help to comment what size of thermal area at 2layer 1oz will be good on this case?
tks for the checking.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
hi Team,
my customer want to use TPS70345 device at 3V3/0.5A, 1V2/1A output use case with 5V input, it is around 3W, would you help to comment what size of thermal area at 2layer 1oz will be good on this case?
tks for the checking.
Hello,
Thank you for your question.
Please allow us 2-3 weeks to get these parameters simulated and get back to you.
Best,
Hannah
Hi Hannah,
update the PCB spec as 6 layer with 1oz.
It is weird that we still not using full load at Output Current Range of 1 A on Regulator 1and 2A on Regulator 2 , why need so long to simulate here?
i purpose it is a roughly 4x4 / 2x2cm area works here.
Thank you for stating the PCB is a 6-layer board. This should be fine with the 1oz copper.
Our thermal simulation team has limited resources; therefore it takes several weeks to complete these requests.
Best,
Hannah
Hi Allen,
The simulation team has stated that there is not enough information to understand what is needed here. The parameters you have provided are too vague and we cannot make assumptions about the customer's PCB layout. Though, we can provide the customer a model of our device for them to use in their own simulations.
Best,
Hannah