Part Number: LM5156H
Other Parts Discussed in Thread: PMP22764
Tool/software:
Hi,
I've designed an isolated flyback circuit, which gets 12V and outputs 56V/600mA.
I used PMP22764 as a reference design, and modified it.
Schematics:
The schematics was already reviewed by Moritz.
Datasheet of the transformer:
I have a problem, that my output is only 10.5V, with no load.
So far I measured:
BIAS =~ 12.1V
EN/UVLO =~ 1.8V
VCC =~ 7V
I've measured the voltage of D22 and I found it to be 4.7V, instead of expected 5.1V (I think I need to make R75 smaller to get higher current).
Please kindly guide me through to debug it. Which information/plots/measurements do you need?
Thanks,
Matan