Tool/software:
Hi,
I'm currently working on enabling the PRECHARGE and PREDISCHARGE modes on the AFE used for our BMS.
Suppose that the PRECHARGE and PREDISCHARGE modes are enabled by setting the related parameters. When there are no faults and no current is flowing through the BMS, the FET status is as follows:
- CHG FET: closed, PCHG FET: open
- DSG FET: closed, PDSG FET: open
My questions are as follows:
-
If the battery starts discharging at a current higher in magnitude than the
Settings:Current Thresholds:Dsg Current Threshold
value, will the AFE immediately open the previously closed DSG FET and close the previously open PDSG FET to perform pre-discharge? -
Likewise, if the battery, whose cell voltage is below the
Settings:FET:Precharge Start Voltage
, starts charging at a current higher than theSettings:Current Thresholds:Chg Current Threshold
value, will the AFE immediately open the previously closed CHG FET and close the previously open PCHG FET to perform precharge?
Thank you,
Kyungjae Lee