Tool/software:
dear T.I.
I have some questions about the output current of the LP5866.
What is the maximum current output from one SW pin of LP5866?
Is it possible to output 550mA from a single SW pin?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
dear T.I.
I have some questions about the output current of the LP5866.
What is the maximum current output from one SW pin of LP5866?
Is it possible to output 550mA from a single SW pin?
Hi Naoki,
The maximum average current that SW can stand is 322mA. If you use LP5866 as 6-scan line, it means you can set the output current maximum up to about 107mA. But if you use LP5866 as 1-scan line, it means you can only set the output current as 322mA/18 = 17.8mA.
Please let me know if there is any other problem.
BR, Jared
Thanks Jared
I have two additional questions.
When using 5-scan lines, what is the maximum current?
The configurable output current is [Maximum average current]*[Number of scan lines]/18, so is that correct?
(Example: When used as 6-scan line, the output current that can be set is 322mA*6/18=107mA)
Hi Naoki,
Yes, your calculation is correct!
The configurable output current is [Maximum average current]*[Number of scan lines]/18, so is that correct?
So, in 5 scan line, the output current can be maximum up to 322mA*5 scan line/18 channel = 89mA. But the maximum output current of CS is 50mA for LP5866, so please don't worry about the current capability of SW.
BR, Jared